Hi,
My customer has an application that requires a very low current consumption temperature switch/sensor, ideally 1uA or less,as it is powered from a coin cell battery. And it has to trigger when the temperature is above 100C. We are considering TMP20.
To save power, we intend to pulse the Vcc of the temperature sensor such that it is 1msec on / 10msec off.
Questions:
- The datasheet has a graph (Fig2) Iq vs Temp at Vcc=5.5V, and another graph (Fig4) on Iq vs Vcc at Temp=25C. We need to know the Iq vs Temp (25C to 150C) at Vcc=2.5V. Can we assume it is similar to !q vs Temp at Vcc=5.5V ? Since the Iq is relatively constant from 2.5V to 5.5V at 25C.
- What is the response time of TMP20 ? ie. When it is powered from 0 to 2.5V, how long will the output be valid ?
- In Fig 10 Thermal Settling, it indicates TMP20 takes about 6 sec to response to a temperature step from 25C to 110C. If Vcc is pulsed with 1msec on / 10msec off, what will be the thermal step response like ?
- We inted to add a MOSFET to the TMP20 output to make it works like a Temp switch such that the output is active low when it is above 100C. Any recommendation on the MOSFET or circuit ?
- Another "brute force" method is to use a pull up resistor ~1Mohm at the TMP20 output to make it look like an active low output. Will it cause any harm to TMP20 ?
Or, is there other better solution to fulfill the low power (~1uA) temperature switch requirement, which will trigger when >100C ? Accurarcy is not so important, but low power is the key factor.
Thanks,
CM.