We're facing an issue with TMP411 with remote temperature measurement. We've used this to measure the junction temperature of Intel IXP processor. Connection details are shown in attached snaps shot
Observation - TMP ALERT/THERM2 pin is never com up if IXP power is switched OFF
We have to cool down the processor junction temperature well below value the thermal limit set in TMP411 , Alert pin never comes up if we don't power down the IXP. ALERT/THERM2 pin will be return back to high state after the junction temperature reaches below set value. ALERT/THERM2 signal is used to control the ON board power supply , once it low all on board power will be switched OFF , only TMP411 power will alive under this conditions
Pls clarify