Hi,
I would like to know if the LM70 (specifically LM70CIMM-5) temperature sensor can operate in a continuous mode with the CS (chip select) pin tied to ground? Only the SI/O and SC pins are connected to the micro, which every 500ms will cycle the SC pin (32 times) and read the temperature from the LM70.
Thanks
John