Hi team,
Regarding to TMP300 temp sensor, I have a question to DWIN.
This is temp switch from -40 to 150. When I set Rtemp 180K for 0'c. Does it output switch only at 0'C? or From -40'C to 0'C?
I meant TMP300 measure only Rtemp point or section with Rtemp point?
If it is for section with Rtemp point, high active or low active?
Thanks in advance.