Hello,
I am looking at an application where LDC1000 would be used in high speed ore (belt application) processing and classification. I would like it know if the drive power level of the LC tank circuit can be increased (to boost sensitivity) and also whether the IC will produce meaningful readings if the ore is moving above the coil circuit (within in a certain time constraint). I am also considering Analog Devices AD5933: (1 MSPS, 12 BIT IMPEDANCE CONVERTER NETWORK ANALYZER), can you suggest why LDC1000 is more suited for this application?
Thanks,
IP