This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH and PCB Coil

Hello,

I am trying to make my own PCB with LDC1000 and
PCB coil using TI WEBENCH application.
The parameters for my design are:

Distance - 0.2 cm
Resolution - 0.2um
Diameter of Target - 2cm
Target material - SS416

The result after export to Altium Designer is  a 4 layer PCB coil which according to WEBENCH should have 4 mil trace width and 4 mil spacing between the traces, but after analayzing the PCB i have 2.852 mil spacing between some of the traces. Тhe difference between the promised and real spacing is a lot more expensive PCB so i am wandering is it a bug or a feature :)