I had some fun with a deck of playing cards. Each card is about .3mm thick and ... pre-numbered! Using an aluminum-alloy base plate and those `gap-setting' playing cards, I entered proximity readings into a spreadsheet and set to trying various conversion formulas to get my 30-sample `distance vs. prox.' chart to make a straight line.
I was thinking it should be some sort of square-law relationship but it seemed that the log() of the prox. readings made a better straight line - up to the point where the gap became close to equal to the loop diameter (where it `took-a-dive' ). Also, the first mm ( three cards) wasn't so good either. Perhaps because the aluminum plate changed the inductance?
*** THE QUESTION(s) *** What IS the theory on the relationship between prox. readings and distance - mathmatically speaking - and have you any suggestions on how to factor in the effect of changes in inductance so as to obtain an accurate up-close absolute distance value?
PS. Rhetorical side-note: There were times when I'd stop my regular pace of measurements to watch the football game for a play or two - and when I resumed, the readings would be offset - a lot. They were going 19000, 16400, 14600, 12700... (pause, watch game for 3 minutes, resume)... 9200, 7500, 6800. Not sure what happened there but it's a little disconcerting to have the readings take a jump for no apparent reason. No - I didn't lose my place - I used numbered cards for exactly that reason. :-) If it happens again - repeatably - in my lab (I was playing on a wooden table in a living room before.) I'll try to provide `less rhetorical' feedback. :-)