Other Parts Discussed in Thread: TMP006
Hello,
I have a question for TMP006.
Q1 : Reduce Object Radius and was wondering how to increase the distance?
I read “TMP006_introduction.pdf” and
“Design Guideline: Place the object a distance no farther than ½ the radius of the object from the TMP006. (d < r/2)”.
I’d like to try to measure d = 1.5 ~ 2[m], and r = 0.15[m].
Please your comment.
Q2 :
Configuration Register : Bit [7] DRDY: Data ready bit
1 = Object voltage and ambient temperature results are ready to read.
“A temperature or sensor voltage read or a write to the Configuration Register is required to clear the condition.”
I’d like to receive easy explanation about “A temperature ~”.
from Eddy(eddy.lee@avnet.com)