Hello,
I am working on a design that will automatically turn a heater on if the ambient temp is below -20degC and turn the heater off if the temp rises above -20degC. Accuracy and hysteresis are not critical parameters, but long term operation and reliability are.
Which is more reliable and robust: a hardware programmed threshold device such as the LM56, or a software programmed threshold device such as something similar to the TMP101?
Thanks,
Aaron