I am trying to incorporate the LDC1000 into a new design, however I have been running into some issues. The LDC1000EVM works fine, however I wanted to replace the coil with a spring and thats when I started to have issues. I do not see any oscillations at INA or INB.
My capacitor is a 100pf ceramic, and these are the characteristics of my spring:
Radius = 0.118 inch
Number of Turns = 15
Height = 0.393 inch
Calculated Inductance = 0.621uH
Measured Inductance (LCR Meter) = 0.761uH
Measured Rs (LCR Meter) = 0.981ohm
Measured Inductance (compressed) = 0.685uH
Measured Rs (LCR Meter/compressed) = 0.893ohm
Calculated RpMAX = 7.182kohm
Calculated RpMin = 1.347kohm
Based on this setup, what would I need to change in the LDC1000EVM GUI to get this working? or do I actually need to modify the LC tank further? If I add series inductance (22uH), I can get see oscillations at INA and INB. However, the change in inductance is extremely small from the spring I have. How small of an inductance could I use to still see oscillations at INA and INB?
Any help would be greatly appreciated.