Hi,
With LDC1000 I can measure a inductive position sensor (one coil with two wires that change inductance with position) between 7mH and 25mH? After, I need a acquisition frequency of 1kHz - 1,5 kHz (in other words, the digital value of inductance in MCU must be updated each 1 ms maximum.
Is possible with LDC1000?
Thanks in advance.
Best regards