I am planning on using the TMP300 for a low power application where the device willl onl be powered on when required. What is the settling period for this device I have assumed that its in the <1ms period. Also I have assumed that the output is active low since it is an open collector configuration so I have assumed that a power up the output will be high (external pull-up ) until the temperature threshold is met- then pulled low. Can anybody help?