This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1000 Drive-by-wire application

On the front page of the datasheet, and in the sales presentation it points out the LDC1000 use for drive-by-wire systems, could you clarify its use for this specific application (only application I can think of is angle sensing). 

thanks

  • Hi Jamie,

    The inductive sensing group mentioned that drive-by-wire can include many applications of position and motion sensing such as pedal rotation sensing, steering wheel rotation, wheel speed, etc.

    Can you please provide more information about the application you would like to target?

    Best Regards,

    Mayrim Verdejo

    Centralized Applications Team (CAT)

    (787)-368-6473

    mayrim.verdejo@ti.com

  • Hi Mayrim,

    Could you please elaborate on what the LDC 1000 has to offer in terms of 1) redundancy and  2) immunity to EMI ? What are the advantages compared to MR or Hall-effect sensors ?  The application is a drive-by-wire electric vehicle. Would it be wise to use these in a traction motor instead of a hall-effect sensor?

    Thanks,

    Darius

  • Darius,

    Let me answer your questions

    1. Could you please elaborate on what the LDC 1000 has to offer in terms of 1) redundancy?

    The working principle of LDC1000 is based on the Eddy Current in the metal. No semiconductor or other high tech materials are involved. Therefore it is the most reliable metal detaction method. In addition, each output is the result of sampling multiple (hundreds or thousands ) times of the Eddy Current induced in the coil.

    2) Immunity to EMI ?

    LDC1000 + Coil as a system is an EM field sensor. It is sensitive to certain EMI circumstances. If the EMI is strong and its frequency is within vacenity of the LC tank frequency, interference can occur. The LC tank frequency is usually low (practivcally 300K to 5MHz). High frequency EMI ususally does not interfere with LDC1000 directly

    Howeer, hi frequency EMI can affect LDC1000 in another way - common mode RF reception by the coil body and cable between LDC1000 and coil. We have experimented with a common mode inductor connected between the coil and the LDC1000. Preliminary result shows that, with the common mode inductantor, the LDC1000 + coil system can widthstand 10V/M EMI from 1MHz to 1GHz. We are developing more effetive EMI mitigations aimed at EMI immunity >70V/M

    3) What are the advantages compared to MR or Hall-effect sensors ?

    The advantages are: a) LDC1000 is totally immuned to static magnetic field; b) LDC1000's sensing element (the coil) is much more robust than the semiconductor materials used in other sensors; 3) Since there is no magnet, there is no worry of picking up metal debris by the magnets

    Best regards,

    Don Liu, Ph.D.

    Tesax Instrument