This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Maximum frequency for LDC1000

What is the maximum allowable frequency of operation for the LDC1000?

I have a tuned circuit with a nominal resonant frequency of 10.5MHz and the LDC1000 seems to resonate at this frequency.  However the datasheet indicates a frequency range of 5kHz to 5MHz, even though the EVM GUI (and datasheet) indicates that it is possible to set a minimum frequency of approximately 12.5MHz.