We are considering using the LDC1000 in our sensor application. The sensor is going to detect openings in an aluminum construction (see attachment). The detector will move along the construction with a maximum speed at 3m/s. There will be two different distances between the sensor and the construction; 2.5mm and 12.5mm.
We are only interesting in the location to the gap in the construction, not the distance to the construction (ie if we have gap or not). Is it possible to detect the edges of the construction with a reasonable accuracy (1/10mm)?
How would you design the sensing coil to gain highest possible accuracy (could a squared shaped coil give a better reading?)