This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CFA, CFB size

Hi,

I read the below in the data sheet:

"Start with a large filter capacitor. For a ferrite core coil, 10nF is usually large enough. For an air coil or PCB
coil, 100pF is usually large enough".

However on the LDC1000 dev board I see it is 20pF? I will be testing air coils with a diameter of ~75mm. Do you suggest I modify this CFA, CFB cap?

Jeff