Hi,
Please tell me the use case to detect the disconnection of the current line
using the LDC1000.
A current flows 500mA at minimum in the line.
But, A current flows 20~30A at maximum.
Specification of the detection coil is unspecified.
There is also no restriction of detection distance.
Does the LDC1000 has ability of detection at these case?
Best regards,