Hi.
The literature and these discussions (and EVM GUI, I believe) seem to be predicated on this formula for the resonant frequency:
f = [1/(2*pi)]*[1/(L*C)]^1/2
But that's not always true, is it?
I believe the resonant frequency of an LC tank this:
f = [1/(2*pi)]*[1/(L*C) - (Rs/L)^2)]^1/2
So that first equation is true only when 1/(L*C) is much greater than (Rs/L)^2 ... but that is not always the case.
Also, does the LDC1000 require 1/(L*C) be much greater than (Rs/L)^2 for the frequency counter to do it's job accurately? I ask because I have a physical L/C tank for which the frequency counter (and GUI inductance measurement) is not accurate. L= 640.5uH, Rs = 222ohm, C = 1000pF. These numbers are good. They were made by independent measurement.
By the numbers this tank should resonate at 191kHz and indeed, I probed the tank (with buffering so as not to significantly disturb the frequency / GUI-measured-inductance) and it is oscillating ~ 187kHz.. Yet f(sensor) from the frequency counter data is 235kHz and the GUI accordingly displays 458uH.
I'd very much appreciate your input.
Thanks.