This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1000 for angular position sensing



I'm looking at the LDC1000 as a potential solution for a small-scale angular position sensor and wondering if anyone could give some feedback on the feasibility, since most TI tools/documentation are focused on distance detection. 

The specifications are:

- 60 degree range

- 0.1 degree resolution

- ~1 to 2 mm distance between coil and target

- ~2 to 3 cm target diameter

Wondering what size coil I would need to achieve this resolution.

Thanks,

Ben Sprague