Hi Team,
I am a student and currently I am working at inductive position sensor, where electronic and sensor are separately because of wet environment and deep temperature. LDC1000 is a great tool for that reason. Ferrite as a coil core is very good material with amplitude about 30% by positioning, almost without any noise. But for my application I can’t take ferrite, then it can be used only till -40 °C, I need it till -190 °C.
Material I am using for coil core and for an opposite target is steel with good magnetic properties. As you know Steel causes eddy currents when dive in a magnetic field, so the LC tank frequency must be lower.
Software, which was delivered with device LDC1000, offers me a function for changing a sensor frequency. In connection with different LC combinations sensor frequency have to influence my amplitude, but when I adjust values by sensor frequency, it changes nothing. Can you explain me how I can take a sensor frequency down? Is it a software error or I overseen anything by adjusting. In general, I mean software works inaccurately and unstable by adjusting all parameters.
Thanks!
Daniel