This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can we use LDC1000 to detect a steel pipe inside a pipe?



Hi, 

We have a client that wants to detect a steel pipe that goes inside another steel pipe. The sensor must be put on the outside pipe. The pipes are 0.5" thick. We were thinking of making the LDC1000 coil wraps around the external pipe and use the minimum LC frequency which according to the datasheet is 5kHz. 

Do you think this is going to work?