Hi all,
I want to make Multifunction Calibrator for my personal use.
Specification for Calibrator (Measure and Generate both) :-
1) mili Volt Range :- 0 to 100 mv
2) mili Amp Range :- 0 to 24 mA
3) Volt Range :- 0 to 30VDC
4) RTD Sensor
5) Thermocouple Sensor
Calibrator will operate with 4.7V battery.
From 4.7V battery to 24VDC and -12VDC.
Looking for Analog Section Schematic, ADC schematic.
If any one can help out in any small part also wellcome.