Hello,
I am in the process of designing my own coil for about 1um resolution. After obtaining the tank circuit, another important parameter which needs to be changed is the CFB Capacitor. However I am unable to obtain proper methods of fixing this capacitor for a changed tank circuit. The datasheet and other discussions in the forum mention that on the CFB pin, a 1V(p-p) is required for the stability of the data & in order to obtain it we need to keep changing the capacitors between those pins and observing the CFB waveform which is highly infeasible . Any Ideas on how to solve this problem ? Also, in the default coil with the LDC1000 EVM, I use a passive probe to test for the signal on the CFB pin and the signl was continuously wobbling, not giving a stable 1V(p-p) waveform. I also tried with a 1kOhm resistor at the input, but with no improvements. Any reason for this ?
With Regards,
Avinash