Dear all,
I have a question about LC tank.
I designed "Original Coil (like Air coil)", then I have evaluated the performance many times with LCR meter.
I have to set LC frequency 200kHz, but Coil inductance value is very large, 50mH.
I'm worrying about the capacitor value very small, it is 12pF at 200kHz.
According to Datasheet, LC frequency is defined from 5kHz to 5MHz. So if LC frequency is satisfied with this range, even though capacitor value very small, the capacitor value is no problem?
Thanks at advance and kindest regards,
Edgard