Dear All,
according the TI expart advices, GUI 1.0.4.1 is better.
Now I'm using ver1.0.4.1, but I can't understand the parameter orders of Log data format.
How in order are the parameters?
For example:
30:06:14:16:04:51:570.000,30276,,30276,
First colum (the forward comma quoted) may be timeline, and next colum may be L inductance value to be calculated.
But I wonder last two parameters "30276,, 32076" may be Rp data which is decoded, but why the same values are appeared? And ", , " is suspicious...
Please tell me that.
Thanks at advance and Kindest Regards,
Edgard