hello,
I need to generate 37 kHz frequency pulses from 28069 piccolo stick. The duty cycle required is 18 %.
Also pulses of 37 kHz, 18% duty cycle with a phase shift of 50% from the previously generated pulses.
Even if i am changing TBPRD, the frequency is remaining 20 kHz only. How do i make it 37 kHz ?