Hi Team,
Whenever I generate a custom coil in Webench and export it to Eagle CAD (v6.4 or later), it generates both a board file (.brd) and a script file (.scr). The board file opens up just fine and shows the dimensions of the coil & C_tank, however when I try to run the script to generate this same coil as a library (.lbr) device it gives me a few errors and only draws C_tank and NOT the coil. This script bug occurs in Eagle v6.4, v6.5, and v6.6.
There is a workaround which I have found which is to use the 'Cut' & 'Paste' options in Eagle to move the coil and cap footprint in the generated .brd file to either my own project .brd file or .lbr file.However, I feel many would benefit if this Eagle script issue could be looked into and possibly rewritten to draw the coil appropriately.
This bug is also referenced in the below post which does not have a reply:
http://e2e.ti.com/support/development_tools/webench_design_center/f/235/t/353773.aspx
Best regards,
Sean