This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

one application of TMP007



Hi BU team

My customer Finisar shanghai site issued an application issue of TMP007 , where TMP007 was in a heat flow meter and monitor the temerature of optical module's shell.  In Ctm's application, thermopile’s ambient temperature may vary from -45 to 80℃. In order to prevent the affection of ambient temperature which could degenerate thermopile’s accuracy. I want to place a TEC  beneath the thermopile(back side of PCB), to stabilize the conjunction temperature. that is to say,

Is this method reasonable?

thanks