We have a coil at 100uH. When we connect different capacitors 30-1800 nF, the coil does not oscillate at the resonance frequency once we go above ~400kHz. The coil oscillates at ~400kHz even if the resonance frequency is 1 MHz. Anything below 400kHz works fine. Any ideas what could cause this?
Off topic: The amplitude configuration 1V or 4V applies to what signal? The CF capacitor, or coil?