Hello,
I am experimenting with the LDC1000EVM to see if it's usable for our application.
We use a coil of 680µH with a ferrite potcore and a capacitor of 1nF, serie resistance of the coil is 6 Ohm.
I changed the CFB Filter capacitor to 680pF to get a amplitude of about 1V PP on the CFB cap
I measured a RP of about 18KOhm.
What i don't understand is that the measured resonance Frequency value is influenced by the RPmin and RPMax setting
Can somebody explain this?
I also see that the signal on the LC resonance circuit is not a full sinewave, at the bottom the sinewave is cutOff, is this normal or should the signal be a full sine wave?