This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

temp sensor

Guru 13485 points
Other Parts Discussed in Thread: TMP006, LM35

Looking for temp sensors with analog interface  for:

1.on Heat sink

2.special place on PCB

3. on copper leads

4.on large cap. of 20mm diameter,35mm long.

  • Hi Eli,

    Let me consult with our SVA team. Will get back to you shortly.

    Mayrim

  • Hi eli,

    All of these can solved with an IR sensor such as the TMP006 and TMP007 but if you want a contact temperature sensor please see below:

    1. The LM35 in the TO-220 package can be attached to any heatsink.
    2. All of our analog sensors can be added to any place on a PCB.
    3. What exactly do you mean copper leads? The LMT8x sensors in the TO-92 package could be a solution.
    4. Same with this, the LMT8x sensors in the TO-92 package could be a solution.

    Please let me know if you have any additional questions.

    -Michael Wong

  • Hi All,

    Thermal IR sensor may be able to address these applications. However both TMP006 and TMP007 are two wire digital interface, I2C and SMBus compliant.

    Regards,

    Werner