Hello.
We are using the TMP122 for years and it has been a reliable solution. The typical temperature deviation is below 0.5°C, however within the last batch we have a cut. The first part is as usual whereas the second part gives temperatures that are 1.25°C higher in average and the deviation is about 0.8°C. We do not reference the absolute temperature but we compare the parts to each other.
Our pcbs are manufactured from another company but they could trace that they changed the reel within this last batch.
On TI's TMP122 page are no errata files listed however we found that there are PCNs. Most likely the parts from the new reel are Rev.A as they were purchased in march 2014. I found out from the PCNs that the changes made in Rev.A are cancelled with Rev.B but there are no reasons mentioned.
Do you suspect that this correllates or is this just random? Can you give me more information about the revisions?
Thank you.
Stefan