This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why is "...difference between RpMIN and RpMAX values reaches x25 - x26.." so important?

Hi TI Team,

there is a famous calibration technique (http://e2e.ti.com/support/sensor/inductive-sensing/f/938/p/298126/1042212.aspx) from Evgeny Fomin, and there in the step 7 is said that "...the difference between RpMIN and RpMAX values.." should not exceed 0x25-0x26. Why is this rule so important?

Best regards,

       Igor Gorbounov

  • Igor,

    There is a difference between 'reaches' and 'should not exceed'. What we are saying, is that the difference should reach a certain amount of codes which translates to a hex value in the register.  

    '' ... OR the difference between RpMIN and RpMAX values reaches x25 - x26, that is your optimal RpMAX setting ".

    The technique is important because you want to use the maximum resolution possible. I hope this clarifies:

    Please, let me know if you have any questions.

    Best Regards,

    Natallia Holubeva
     
        
      
      
      
      
      
      
      
      
      
      
      
     
     

  • Hi Natalia,

    I see now that I've made a mistake in my question: the difference sholdn't be LESS than 0x25-0x26.

    Now I see from your answer that this is somehow related to measurement technique - perhaps

    when this difference is small the measurements are noisy. I ask this only because there is no

    official appnote with calibration method released yet, though several times promised.

    Thank you for your answer.

         Igor Gorbounov

  • Hello Igor,

    We are working on it. I apologize for the delay.

    Best Regards,

    Natallia Holubeva