This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1000 / relationship between coil diameter and target diameter

Guru 20090 points

Hello,

Could you please let me know the relationship between coil diameter and target daiameter?

I understood that the detect distance is the half of the coil diameter for high resolution sensing.
Also I understood that the inductance coil size is limited by Rp.
Thus, if we use the coil which has large diameter and low inductance expands the detect distance.
However, I think that there is the suitable coil diameter for each target size.

Best Regards,
Ryuji Asaka