This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1000 without INTB Functionality

I want to use LDC1000 for Linear position measurement. But I don’t have any extra GPIO for INTB Pin.

When I checked the LDC1000 datasheet, there is a mode for disabling INTB functionality.

This can be achieved by setting Field  “Mode” in  “Address = 0x0A” to value  “000: All modes disabled”

I am not sure that it will impact the functionality/working of sensor. Will I be able to read the position from sensor with regular SPI configuration (without INTB)?

regards,

yogesh