This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About resister writing of LDC1000

Guru 19645 points

When resister writing to LDC1000, nothing is sometimes written in.

Can some cause think of?

I think there is timing until begin to write after a power supply is turned on.

When it's right, please tell me the this time.

------------------------------------------------------------------------------------

【Additional information】

・PWR_mode is "Stand by". (No problem)

・Customer don't use CSB pin. (Controlling one LDC1000)

・Procedure

  ・Power supply on

   ↓

  ・Initialization

   (1) RpMAX (0x01)

   (2) RpMIN (0x02)

   (3) Min Resonating Frequency (0x03)

   (4) Amplitude & Response Time (0x04)

   (5) PWR_Mode:Active mode set (0x08)

------------------------------------------------------------------------------------

 

Best regards,

Satoshi