This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007 output timing

Hello,

My customer uses the TMP007 and has a question.

He wants to know the temperature of a object after power on, ASAP.

How many seconds does it take it output a temperature data after power on?

Regards,

Naoki Aoyama

  • Hi Naoki,

    We will get back to you on this tomorrow.

    Best Regards,

    Mayrim

  • Hi Naoki,

    If the customer is powering the device off then powering the device back on, the TMP007 will initate a power-on-reset each time the power is re-applied.  This will return the TMP007 to its defaut register settings.  On default the TMP007 will power up in a continuous conversion mode with the conversion rate set for 1.01 s total conversion time.  Therefore it will take just over 1 s before the first conversion is completed.  As an alternative the customer can use the non-volatile memory to change the configuration register settings.  iI for example they would like to reduce the conversion time to as low as 260 ms.

  • Hi Edward,

    Thank you for your reply.

    I will feedback to my customer the information.

    Thanks

    Naoki Aoyama