I am evaluating the performance of TDC1000. Can you give the source code of TIDA-00322 on C2000 processor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am evaluating the performance of TDC1000. Can you give the source code of TIDA-00322 on C2000 processor?
I have submitted an update to the TIDA-00322 software that includes the firmware source code zip. It should post on the TI web in the next few days.
Firmware hex file (TDC1000_C2000_FW-v1.42-1MHz.hex) is in the install folder C:\Program Files (x86)\Texas Instruments\TDC1000_C2000\Firmware where the source code zip is also there.
You have to use CCS and import/open the projects. "TDC1000_level_PC_Commn" is the project to use to build the code.