hello,anyone. recently, i am working with the temperature sensor PT100. the temp range is 0-100 degrees celsius. and i want the output is 4-20mA. and i find that the XTR105 is a good selection for my project. but i find that the temp range of XTR105 is -85-125. so i donnt konw how to configure the IC. can anybody give me some suggestions. Again: temp range:0-100 degrees celsius, output 4-20 ma. thank you.