Hello Team!
I have a quick question that I just want to run by you to make sure.
According to the datasheet, the internal clock frequency ranges from 35 MHz to 55 MHz, and then varies also with temperature.
Does this mean that any one part may have its internal clock vary over that range with constant temperature, or that the part to part frequency will vary over that range?
Do you know how stable that frequency is? For example, if a part has an internal clock frequency of say 45 MHz at a given temperature, will it be 45 MHz +/- 1% if there is no temperature variation?
Thank You,
Michael