I realize this isn't the classic application for these chips but please if you could think outside the box a little I think they might have application to my needs.
I want to detect the location of an impact on a steel mounting plate via TDOA with 4 piezo sensors. So I don't think there needs to be any "transmission" from the AFE because the impact will provide the signal.
What I'm thinking is continuously (or every x mS) triggering the start signal and then when an impact occurs measure the "time of flight" to each of the sensors. By using 4 sensors we can use the first reception as zero time and difference the arrival of the signal to each of the others. The time from the start signal doesn't matter only between the times of arrival at each sensor.
Does this make sense? Seems like there is a lot of precision timing and analog stuff in these chips that can be used. I realize I might have to use two chips to interface to the 4 sensors.
Thoughts appreciated.