Other Parts Discussed in Thread: LDC1000EVM
Hi
We have made a coil based on the old webbench tool.
I am not able to reproduce the results in the new tool. Why is this?
Our coil is 51mm, has 2 layers of each 115 turns.
In the first design the webbenchtool suggested using a 22pF capacitance, but the new design guidelines indicate that this is below minimum:
Also the new tool has a lower limit of 50pF.
I must say that the 22pF cap works very well in our setup, so I just wanted to recreate that setup in the tool but the tool.
The old tool does not even give me altervatives for the LDC1000, only for the 1612 and the 1614.
http://webench.ti.com/webench5/ldc/index.cgi?d=4.5&res=999&td=3&tm=2&resolutionBasis=l
Any thoughts on this?