Please clarify which EVM module will be the correct one to purchase.
- I will be using a single transducer and single temperature sensor.
- I will be testing the transducer at distances up to 20 feet. This means I will be measuring a distance of 40 feet.
- Both descriptions of the EVM modules are close with the exception of the use of the TDC7200 INTEGRATED CIRCUIT.
- I am hoping to evaluate different ultrasonic transducers on the tanks.
- Is one of the two EVM's a better selection.
- The TDC1000-TDC7200 seams to test more features however I noticed that the TDC1000-C2000 has a selection tab which says tank level. Does this mean the TDC1000-C2000 is the better selection?