With a proper transducer, can the TDC1000 be used to measure TOF in a metal medium (e.g. rod)? Propagation speed is appx. 0.177 inches/microsecond. Pulse center frequency would be 39KHz. Reflected pulse would vary based on the position of a magnet which induces a strain in the rod (magnetostriction effect).
Is there another part that would be better suited for such an application?
Thanks.