Hello,
I am using TDC-1000-GASEVM and TDC1000-BSTEVM to observe the amplified 30V output from the HV Board. On connecting the probes to the Start and the TX1 pins of GASEVM board, I can observe start pulse and 3.7V square wave on the Oscilloscope. But when I connect the HV board to the TDC-1000-GASEVM board and check the output, the 30V signal doesn't come up. Are there any specific parameters to be set in the software to achieve the 30V output?
I have set the following parameters:
CPU_CLK FREQ: 1MHz
TDC1000-HV Driver EN1: Checked
EN1 Period: 30 us
TDC1000-HV Driver EN2: Checked
EN Period: 15 ms
TDC1000-HV Boost Power Enable EN: Checked
Also, I can observe the enable signal on VDD_EN1 pin and the EN_Boost pin of the HV board but nothing comes out of the TP2 (30V) pin.
Also, can that be because the HV board is faulty? Is there any way to check that? Please suggest me how to debug this issue?