Smooth change in the distance between the object and the coil leads to a step change of Rp near the value 16384. Disign parameters:
coil diameter 19mm - made of 19-turn winding wire; coil capacitance: 100pF reg. settings: Rp_MAX = 0x1A; Rp_MIN = 0x3F Sen_Freq = 228 LDC_Conf = 0b00010111
The figure shows the result of measurement Rp codes (period 500us) with a smooth, almost linear, change in the distance to the target. Has anyone have met something similar?