I am using HDC1008 (200pcs)assembly our products,Temperature accuracy is good, but the accuracy of humidity is higher 6~8%, why?Is it necessary to open the heating function for reduce humidity ? In that way temperature is error .so I'm going to subtract 7% of HDC1008 readings, But in this wayour products 's max humidity is only 93%.Is there any method to read HDC1008 data over 100% ?