I recently purchased a MSP-FET to work on the TDC1000_TDC7200 EVM board. I have confirmed that the MSP-FET by using the MSP FET to download a few of the demo program to MSP430FR5969 Launchpad.
I also have populated the JTAG header J1 so I can connect the MSP-FET. I connect the MSP-FET to the TDC1000_ TDC7200 board with the white marked wire side close to the USB connector.
I have identified that the TDC1000_TDC7200 board has a MSP430F5528 micro controller.
I am trying to program to blink the LED on P4.5 just to confirm that the set up is working accurately. The issue is when I try to program the part I get the following error.
Error initializing emulator: The voltage 1119 value is not correct/allowed for the USB FET
Appreciate if someone can shed some light on the error.
Thank you.