This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please elaborate on the temperature sensing accuracy testing method used for verifying the temp sensing accuracy specification(<+/-0.75degC) for the LM35 part? Basically accuracy would be the difference between the actual/reference temperature and the temperature readout as per LM35 output right. How was the temperature forced over the device? Was a thermostream approach used (eg www.temptronic.com/.../ThermoStream_Overview.htm), or was a peltier based approach used(eg www.mechanical-devices.com/.../PageGen2.asp)? www.grantinstruments.com/.../1._high_temperature_oil_baths___circulators.pdf, us.flukecal.com/.../6330732073407380-comp-0)?
Thanks,
Anoop
Hi Michael,
Thanks for the confirmation. The application was actually to check the accuracy of one of our temperature sensors, so we wanted to verify the accuracy of our temperature forcing mechanism using a good reference temp sensor like LM35. I was interested in LM35 because of the easy temperature read out method using just an output voltage, rather than a digital readout, which results in a simpler board, I couldn't locate another temp sensor with voltage output with better accuracy.
Can you also please let us know the name of the oil path unit used by you if possible
Thanks,
Anoop
Hi Anoop,
You are correct, the LM35 output is easy to read, unfortunately its accuracy is only +/-0.5C at room temp. We have a new part out, the LMT70, which has +/-0.13C (max) accuracy at room temp and +/-0.36C (max) over the full temperature range of -55C to 150C. This part is also an analog output sensor, to convert to temperature use the look up table in the datasheet. We like the Fluke oil baths.
-Michael Wong
Hi Michael,
Thanks for the suggestion, LMT70 appears awesome, unfortunately we have already released the LM35 board for fabrication, will plan to incorporate LMT70 in the next revision
Thanks,
Anoop