Hello
In our application there is a distance of 10 cm between the 4 sensors and the FDC1004. We have wired it with a coax calbe using the Active Shield, as shown in Fig. 6, chapter 3.1 Single-Ended Measurement in the document 'Capacitive Sensing: Ins and Outs of Active Shielding' (SNOA926A). But the result is, that the influence of a hand can be seen in the result. Why?
What about the Ground? In the document, as well as in the manual, the GND routing is not specified. If the sensor is on the same PCB as the IC, it is obvious. But if the sensor is connected with a wire - so we have installed a separate GND wire between every sensor and the SHIELD1 pin of the IC. Is that correct, or shall we shield the GND also?
Best regards
Alois